Use Variables in Programs
| Using variables in programs |
Structs, which are complex data types, are not supported in application variables. Communication handler objects (e.g. xmlrpc, ros_subscriber, etc.) are not supported as application variables. Application variables can be used in the same way as any other variables in the program. They are added to a list of variables available in the dropdown lists.
See the variables inside the blue box in both the main screen and the multitask screen. Information found in both screens correspond to each other.
|