Saving Variables
| Saving variables |
Each program in PolyScope X has its own set of application variables. Variables are saved to the internal program database when program is stopped and automatically every ten minutes. Every time a program is switched, all variables are cleared and replaced with variables defined in the newly loaded program. When a program is loaded again, values of Application Variables are automatically restored to the last state. See the switch of the application variables between the programs “Pick and Place final” and “End Effectors.”
Pick and Place final program screen
End Effectors program screen
|