<link rel="stylesheet" href="app_assets/styles-R77XALWP.css"> Skip to main content

Automated Screwdriving for Automotive

Automotive assembly requires fast, repeatable, and traceable screwdriving & bolt driving across interiors, seating, electronics, and other sub‑assemblies. Universal Robots cobots automate screwdriving tasks with precise torque control, fast changeovers, and collaborative safety, supporting OEMs and Tier suppliers alike.
04_2021_Lear_Corporation_Case_Story 1 screwdriving

Advantages of Automated Screwdriving with Teradyne Robotics

Manual screwdriving in automotive assembly often limits takt time and can introduce quality variability across shifts and models. Multiple process locations in close proximity, tight tolerances, and ergonomic strain make sustained consistency difficult at scale. Quality challenges can drive fines from the OEM, stop production lines or create costly manual inspection requirements on the supplier.

UR collaborative robots deliver controlled force, speed, and positioning to ensure every fastener at every stage of the process is driven to specification—without slowing production or increasing operator risk. And UR collaborative robots are more easily deployed than traditional automation as a six sigma, kaizen, or lean continuous improvement project on existing production lines and workcells.

Why Automate Screwdriving in Automotive Assembly

Manual screwdriving is repetitive and difficult to standardize across shifts, operators, and vehicle variants. In automotive environments where access is limited and cycle times are tight, fastening variability can quickly affect throughput and quality.

Collaborative robots paired with integrated screwdriving tools allow manufacturers to control force, speed, and position at every fastening point. This ensures each screw is driven to specification while supporting a stable, repeatable production flow.

Key outcomes include:

  • Precise torque and depth control for repeatable fastening
  • Fast changeovers support mixed‑model automotive production
  • Reduced ergonomic strain for operators
  • Integrated verification supports quality and traceability
  • Collaborative operation without heavy guarding
Screwdriving application in Automotive

"It was an extremely rapid deployment that took us between 2 and 3 months."

FiRAC simulates real-life automotive assembly line conditions to advance screwdriving applications

In a robotic screwdriving setup, the collaborative robot guides the screwdriver to each fastening point with high positional accuracy. Force, speed, and insertion depth are monitored throughout the fastening cycle to ensure compliance with engineering specifications.

Because the robot operates safely alongside operators, automated screwdriving can be deployed directly at existing assembly stations. This allows manufacturers to automate fastening tasks without re‑engineering the entire cell or introducing rigid safety barriers.

The result is a more predictable fastening process that supports just‑in‑time assembly while reducing variability and ergonomic strain across the line.

Discover FiRAC complete case story.

Automated ScrewdrivingNut running requirements vary depending on torque range, accessibility, and tool integration. Collaborative robots used in automotive fastening are typically selected based on their reach, payload, and ability to support precise torque‑controlled tools.Nut running requirements vary depending on torque range, accessibility, and tool integration. Collaborative robots used in automotive fastening are typically selected based on their reach, payload, and ability to support precise torque‑controlled tools.

Selecting the right robot for automotive screwdriving

Compact UR cobots are well‑suited for automotive screwdriving tasks where reach, speed, and repeatability are critical. Their lightweight design enables fast repositioning across workstations, while built‑in force control ensures consistent fastening without over‑tightening or part damage.

Related automotive assembly applications

Automotive assembly requires fast, repeatable, and traceable screwdriving across interiors, electronics, and sub‑assemblies. Universal Robots cobots automate high‑mix screwdriving tasks with precise torque control, fast changeovers, and collaborative safety, supporting OEMs and Tier suppliers alike.

Automotive Nut Running

Automotive Nut Running

Screwdriving and nut running are often deployed on the same stations or adjacent stations and are evaluated together as fastening strategies.

Automotive Clip Insertion

Automotive Clip Insertion

Automated clip insertion for interior and exterior assemblies, improving consistency and reducing part damage.

Automotive Press‑Fit Assembly

Automotive Press‑Fit Assembly

Robotic press‑fit operations for controlled insertion of bearings, bushings, and precision components.

Automotive Parts Transportation

Automotive Parts Transportation

Automotive manufacturing relies on a continuous flow of materials. Components, kits, and containers need to reach the correct station precisely when required to ensure takt time and stable production.

josephine payne ford romania engine plant manager

Ford Dagenham Enhances Engine Production with Universal Robots

Ford Dagenham deployed seven UR10 robots to automate engine fastening, replacing a manual task. Operating 24/7, the solution handles engines arriving every 30 seconds with consistent precision.

By automating this repetitive process, Ford improved productivity, reduced costs, and eliminated operator strain, while ensuring reliable, high-quality results across the production line.

Explore next steps in automotive applications

Talk to an automotive automation expert

An automotive automation specialist will follow up to discuss your application and production requirements. The goal is to understand your setup and explore practical automation options, no commitment required.