Password - Admin

Description

All options under Security are protected by an Admin password. The Admin password protected screens are locked by a transparent overlay rendering the settings unavailable. Accessing the Security allows you to configure the settings in the following:

  • Secure Shell

  • Permissions

  • Services

The settings can only the modified by designated administrator/s.

Unlocking any one of the options under Security, also unlocks the other options until you exit the Settings menu.

 

Default Password

The default password for the admin password is: easybot

If you forget your admin password, it cannot be replaced or recovered.

You will have to reinstall the software.

To set the Admin password

Before you can use the Admin password to unlock protected screens, you have to change the default password.

  1. Access the Hamburger menu and select Settings.

  2. Under Password, tap Admin.

  3. Change the current Admin password to a new one.

    • If this is the first time, change the default Admin password from "easybot" to a new password. The new password must be at least 8 characters long.

  4. Use the new password to unlock the Settings menu and access the options under Security.

 

To exit the Settings menu

When one of the Security options is unlocked, the Close button in the bottom right of the Settings menu changes. The Close button is replaced by the Lock and Close button indicating security is unlocked.

  1. On the Settings menu locate and tap the Lock and Close button.