|
The Safety Checksum icon displays your applied robot safety configuration. The checksum changes if and only if the safety configuration is changed.
The icon has three states/appearances:
-
A hand indicates that the control station is in control and the operational mode is set to manual.
-
A whirling process indicates that the control station is in control and that the operational mode is set to automatic.
-
A remotely connected system indicates that control is external to the station.
Safety Checksum is the only menu with non-labeled icon .
The Safety Overview screen is divided in two:
|