Main Navigation

Description

The main navigation, also called the navigation hub, contains five settings/menus:

  • Hamburger menu icon

  • Application

  • Program

  • 3D Viewer

  • Operator Screen

More about the Main Navigation

When you open PolyScope X, your main screen is by default the Operator Screen.

The Operator icon, highlighted in blue, indicates this.

 

 

When you tap an icon, it is highlighted blue in the main screen, which indicates it is active. The hamburger icon is an exception to this.

Tap

hamburger

icon

Tap Application

Tap Program

Tap 3D

Tap Operator