Automatic Operational Mode

Description

In Automatic Mode, the robot can only execute a program of predefined tasks. You cannot modify or save programs and installations. This has two properties:

  • Automatic program execution is allowed

  • Motions at full speed (complying with safety limits)

 

To use Automatic mode

  1. Follow the steps of “To access Mode Selection” in Operational Mode. See Operational Mode.

  2. Tick the Automatic button in the Select Operational mode, enter the operational mode password to unlock, and Confirm.

    While in automatic mode, the PolyScope X interface is in the operator screen and the tabs in main navigation and sidebar are reduced. Additionally, the automatic mode icon is displayed above the Safety checksum .

     

  3. You can tap the Play button in the footer or the robot control bar.