System Manager

Description

The System Manager enables you to do the following functions:

  • See all created programs and installed URCaps

  • Create a new program

  • Import programs

  • View script of selected program

  • Write a program description

 

To access System Manager

There are two ways to access the System Manager: via header and via hamburger icon.

Header. Tap the header, which contains solely the Program name menu.

Hamburger Icon. In the main navigation, tap the hamburger icon and then System Manager.

 

 

 

The System Manager screen appears, which contains the following components located in three columns.

 

 

On the left column are found the Program section and URCaps section.

On the center column are found the Program Manager, which lists the created program, and the + Program button/icon, which enables the creation of new program and importing a program.

On the right column are found the editable Description field and View script button.