Program Menu

Description

The Program menu gives you access to the commands and clipboard toolboxes, which contains the basic command nodes.

 

To access Program

When you tap the Program icon, the Main Program screen becomes the main screen. The active program is seen in it, along with the details of the command nodes used in the program tree.

Tap the add icon to access the Commands and Clipboard toolboxes. See Command Nodes.