Articles Download Safety & Security Forum myUR Go to Main Site

Universal Robots A/S
Energivej 51
DK-5260 Odense S

T: +45 8993 8989
sales@universal-robots.com

 
  • Articles
  • Download
  • Safety & Security
  • Forum
  • myUR
  • Go to Main Site
  • Support
  • Articles
  • MINIMIZE COORDINATE DIFFERENCE

MINIMIZE COORDINATE DIFFERENCE

This describes strategies to minimize coordinate differences when programing applications.

Last modified on Feb 24, 2025

Created: December 6th, 2024.

New features introduced in Polyscope 5.16 added URScript functionalities that allow treating frames as objects. This enables the relocation of frames to new poses and referencing of frames to other frames. These features allow for corrections over setups that have been modified and enable recalibrating the entire program in case of a loss of precision. 

Some case examples are presented below to illustrate the possibilities of using these features: 

 

Case 1: Trajectory Referenced from a Custom Frame 

Teaching and using frames of reference, features, closer to the path points reduces deviation since there is less distance involved. The image bellow compares relative position against custom feature and base feature, while the robot is in the same position, same joint values. Using custom frames help to reduce relative errors in non-calibrated robots. 


Examples: 

  • Module 10 : Module 10 ELearning explains and guides over the use of custom frames to reference points. 

 

Case 2: fast reconfiguration of Trajectory Referenced to A Frame 

By creating a new frame (e.g., table) using the add_frame(name, pose, ref_frame="base") function, and creating points as frames referencing and attaching them using attach_frame() (e.g., cornerA, cornerB) to the first frame (table), whose pose can be referenced to either the robot's base frame or the world frame, we can easily update the program's motion. This is achieved by simply reteaching the frame's position, move_frame(name, pose, ref_name), relative to its parent frame (world or base) if the robot's position has changed or the trajectory has shifted due to changes in the work environment, such as the table being moved by a general offset.

This also provides a method to reduce deviations from the trajectory in non-calibrated robots. Teaching and using a frame of reference close to the path points reduces deviation since there is less distance involved.

Examples: 

  • Adding, Moving, and Attaching Frames

  • Module 10 : Module 10 ELearning 
     

Case 3: Use of Fiducial Markers to Enhance Precision 

Fiducial markers are tools used in the electronics industry to reconfigure trajectories and avoid deviations in component placements. A similar strategy can be applied using fixed points in a robot application setup. A program with a 2D or 3D trajectory can reference a specific point, such as the midpoint of two, or more, fiducial markers, to improve precision. That point can be located by interpolation. For this approach, the interpolate_pose() function is used. 

Steps: 

  • Set two, or more, physical points to act as fiducial markers over the work set up or the item to work upon. 
    add_frame(markerA, pose, ref_frame="base") 
    add_frame(markerB, pose, ref_frame="base")

    These two points might have a physical fixed reference on the work environment.

  • Define a reference point relative to these fiducial markers to set the reference frame for all the other points, and to be checked at the beginning of the program, e.g. corner of the piece or work environment.
    add_frame(referenceFrame, pose, ref_frame="base")
     

  • Every time the program starts, if the verification of the reference point fails, use the interpolation function to adjust the frame based on the physical fiducial markers: 
    referenceFramePos = interpolate_pose(markerA,markerB, i)
    move_frame(referenceFrame, referenceFramePose, ref_name = "base")

    i is the index that indicate the position of the referenceFrame along the line from markerA and markerB, this should be determine at the planification of the application. More than two markers are necessary for points that lies outside of the segment markerA-makerB or in 3D space. Check Interpolate a square or lattice using scripts.

Related articles

Examples of Script Commands
URScript: Dynamic Force Control
URScript: Move with respect to a custom feature/frame
TCP/IP socket communication via URScript
Interpolate a square or lattice using scripts
Interpolate a position using script
logo

Product

  • UR3e Robot
  • UR5e Robot
  • UR10e Robot
  • UR16e Robot
  • UR20 Robot
  • UR+ Products

Company

  • About us
  • Contact us
  • Careers We're hiring
  • UR merchandise

Training / Resources

  • Academy
  • Technical Resources
  • Articles
  • FAQ

Insights

  • Blog
  • Content library
  • News centre
  • Podcast
  • Webinars & Events

Get in touch

  • Ask an Expert
  • Schedule a no-cost assessment
  • Find a distributor
  • Customer support

Connect with us

  • LinkedIn
  • Facebook
  • Twitter
  • YouTube
  • Instagram
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com
  • Copyright @ Universal Robots 2026
  • Cookie policy
  • Privacy policy
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com

Copyright © Universal Robots 2026

Cookie policy
Privacy policy