Articles Download Safety & Security Forum myUR Go to Main Site

Universal Robots A/S
Energivej 51
DK-5260 Odense S

T: +45 8993 8989
sales@universal-robots.com

 
  • Articles
  • Download
  • Safety & Security
  • Forum
  • myUR
  • Go to Main Site
  • Support
  • Articles
  • Insufficient storage for a PolyScope X urup update

Insufficient storage for a PolyScope X urup update

Last modified on Oct 23, 2026

Use this procedure when a software update cannot be installed because the SD card does not have enough free space, and the current programs, settings, and URCaps must be kept.

Products affected: PolyScope X cobots that boot from an SD card (CB5.6).

A PolyScope X system image leaves most of the card for the data partition. On the first boot that partition is expanded to fill the card, and the expand runs only that once. Copying the card onto a larger one keeps the old partition size. The extra capacity stays unused until the expand is enabled again.

Other options

  • Delete data that is no longer needed, such as unused URCaps, and then run the update.
  • Install a new image of the target version, then install URCaps again, reapply settings, and import programs.

SD card

Use a Class 10 card of the same quality as the card supplied with the robot. A slower or poor-quality card can cause unstable operation and degrade performance. The new card must be larger than the card currently in the robot.

Before you start

  • Power off the control box before removing the SD card.
  • The computer used for the copy needs free disk space for a full image of the current card.
  • Keep the original card until the new card has booted and the update has finished.
  • The commands below overwrite the target device. Copy the whole card. Do not copy a single partition, and do not use a tool that resizes partitions during the copy.
  • The instructions here are for performing the copy from a Linux terminal. On other operating systems, it requires third-party software, such as Balena Etcher or Rufus.

Procedure

  1. Power off the control box and remove the SD card.
  2. Insert the card into a computer. Identify the whole-disk device with lsblk. It must be the disk, for example /dev/sdX or /dev/mmcblk0, not a partition such as /dev/sdX1.
  3. Write the card to an image file:
    sudo dd if=/dev/sdX of=polyscope-x.img bs=4M status=progress conv=fsync
  4. Remove the original card. Insert the larger card, check the device name again, and write the image to it:
    sudo dd if=polyscope-x.img of=/dev/sdY bs=4M status=progress conv=fsync
  5. Insert the larger card into the control box, connect power, and start the robot. Wait until PolyScope X is up.
  6. Attach a keyboard to a USB port on the CB5.6 and press CTRL+ALT+F1 to get a terminal.
  7. Log in to a terminal as root and with the password to the cobot.
  8. Run this command to enable expanding the filesystem:
    systemctl enable expand-on-first-boot.service
  9. Reboot the robot with:
    reboot
    On that boot the data partition is expanded to fill the card. The service then disables itself. A later reboot does not expand the partition again.
  10. Run the software update as usual.
logo

Product

  • UR3e Robot
  • UR5e Robot
  • UR10e Robot
  • UR16e Robot
  • UR20 Robot
  • UR+ Products

Company

  • About us
  • Contact us
  • Careers We're hiring
  • UR merchandise

Training / Resources

  • Academy
  • Technical Resources
  • Articles
  • FAQ

Insights

  • Content library
  • News centre
  • Podcast
  • Webinars & Events

Get in touch

  • Ask an Expert
  • Schedule a no-cost assessment
  • Find a distributor
  • Customer support

Connect with us

  • LinkedIn
  • Facebook
  • Twitter
  • YouTube
  • Instagram
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com
  • Copyright @ Universal Robots 2026
  • Cookie policy
  • Privacy policy
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com

Copyright © Universal Robots 2026

Cookie policy
Privacy policy