Roberta Nelson
Roberta Nelson Shea is the Global Technical Compliance Officer at Universal Robots responsible for product safety and reducing barriers to global acceptance and deployment.
She has already spent 34 years as a professional within the field of manufacturing automation, 23 of them additionally chairing the US-American National Robot Safety Committee. She has also been elected one of the top 100 Women in Safety by the American Society of Safety Engineers (ASSE). As chair of the ANSI/RIA R15.06 she has developed and defined various technical standards for industrial robots. Most recently, as chair of the committee ISO/TC 299 (ISO/TC 184/SC2), she lead the introduction of ISO/TS 15066, which, as an extension of the established ISO 10218, is the first document defining standardized safety requirements within human-robot-collaboration.