System

Description

The system settings contain underlying settings that is set once and very rarely changed.

 

 

Languages

You can change the preferred language for the UI.

Tap the Language drop-down menu and find your language.

 

Theme

You can choose between Light and Dark user interface theme.

 

Units

It is possible to change the precision of the software in the settings. Please make sure that you verify this setting, before you start programming the robot program.

 

Angle Units:

You can change between degrees and radian.

 

Mass Units:

You can change between kilogram and gram.

 

Length Units:

You can change between meter and millimeter.