Controller I/O
| Description |
Controller I/Os are the electrical signal interfaces on the robot's Control Box that allow the robot to communicate with external equipment such as sensors, switches, relays, PLCs, conveyor belts, lamps, etc. All controller I/O signals are prefixed with "CB_".
The illustration below shows the layout of electrical interface groups inside the Control Box. Observe and maintain the color scheme as illustrated below. |
|
| Digital I/O specification |
The digital I/Os are constructed in compliance with IEC 61131-2. The electrical specifications are shown below.
*For resistive loads or inductive loads of a maximum of 1 H.
|