Mounting and Connecting

Description

Mount the Control Box and Teach Pendant correctly and assemble them with the Robot Arm to ensure stable installation and reliable system setup. Securely install and connect all components according to the specified requirements to prepare the system for PolyScope X.

 

 

Mounting and operating the robot in environments exceeding the recommended IP rating can result in injury.

Unstable mounting can result in injury.
  • Always make sure the robot parts are properly and securely mounted and bolted in place.