System

Description

The system settings contain underlying settings that is set once and very rarely changed.

 

 

Languages

You can change the preferred language for the UI.

Hit the language selector and find your language.

 

Theme

You can change the preferred language for the UI.

Hit the language selector and find your language.

 

Units

It is possible to change the precision of the software in the settings. Please make sure that you verify this setting, before you start programming the robot program.

 

Angle Units:

You can change between degrees and radian.

 

Mass Units:

You can change between kilogram and gram.

 

Length Units:

You can change between meter and millimeter.