Robot Limits
| Limits |
|
|
| Safety Mode |
Restricting stopping time and distance affect overall robot speed. For example, if stopping time is set to 300 ms, the maximum robot speed is limited allowing the robot to stop within 300 ms. The tool speed and force are limited at the tool flange and the center of the two user-defined tool positions Under normal conditions, i.e. when no Robot stop is in effect, the safety system operates in a Safety Mode associated with a set of safety limits 1:
|