Smart Skills
| Description |
Smart skills are quick-access robot actions that you can start and stop to achieve a smoother and faster programming experience. Through these actions, you can manipulate the robot, any external systems, or end effectors. These are the Smart Skills to choose:
Activated Deactivated
|
| To access Smart Skills |
There are two ways to access Smart Skills:
|
| Access via Move section |
Via Move section is where you press and hold the button on the teach pendant while the smart skill is executing. The corresponding robot movement is seen in the main screen.
|
|
| Access via Application tab | Via Application tab is where you can configure and set up the input arguments.
|
‘