Align to Plane

Description

Align to Plane assists you in orienting the TCP to a surface. While executing this smart skill, the robot will touch up 3 (default value) points on the surface from which it computes the plane’s orientation. The contact points are laid out in a circular pattern which has a default diameter of 2.5 mm. This smart skill is especially useful for creating new frames in the Frames application.