Profinet

Description

The PROFINET network protocol enables or disables the connection of the robot to an industrial PROFINET IO-Controller. If the connection is enabled, you can select the action that occurs when a program loses PROFINET IO-Controller connection.

 

Enable Profinet

This is how you enable to Profinet function in PolyScope X.

  1. In the top right of the screen, tap the Hamburger menu and then tap Settings.

  2. In the menu on the left, under Security, tap Services.

  3. Tap the Profinet button to switch Profinet on.

 

 

Using Profinet

Find the profinet functions in PolyScope X:

 

In the PolyScope X left header.

  1. Tap the Application icon.

  2. Select Profinet from the left menu.

Select the relevant action from the list:

Ignore

PolyScope X ignores the loss of Profinet connection, and the program continues to run.

Pause

PolyScope X pauses the current program. The program resumes from where it stopped.

Stop

PolyScope X stops the current program.