<link rel="stylesheet" href="app_assets/styles-R77XALWP.css"> Skip to main content

Robotic Picking

Automate how parts are picked, verified, and delivered
Collaborative robot arm performing automated picking in a warehouse with organized storage bins

Robotic Picking for End‑to‑End Material Flow

Robotic picking changes how materials are handled across production and fulfillment operations. Instead of relying on manual retrieval, robots perform picking tasks with consistent accuracy while autonomous mobile robots keep materials moving safely between stations. Universal Robots and MiR work together to connect precision picking at the workstation with autonomous transport across the facility—creating a continuous picking and fulfillment workflow.

Robotic picking uses collaborative robots to identify, retrieve, and place parts with repeatable precision, including:

The result is consistent picking performance, regardless of product mix, shift changes, or operator variability.

Core Robotic Picking Workflows

application material handling dcl

Robotic Picking Customer Success

At DCL Logistics, UR cobots were deployed in a fulfillment environment to automate picking and packing workflows. The system integrated directly into existing processes and enabled significant improvements in efficiency, labor utilization, and order accuracy—demonstrating how automation at the consolidation and packing stage is critical to scaling high-volume picking operations.

What we’ve seen is up to a 500% increase in productivity by using the robot. The ROI on the robots so far has been three months.

Dave Tu, President. DCL Logistics
Case Story Tomenson Machine Works 12

Combining UR and MiR for a Complete Robotic Picking Solution

Universal Robots: precision picking, sorting, and kitting MiR: material flow, transport, and coordination

Together, they:

  • Remove manual transport steps
  • Improve pick accuracy and consistency
  • Maintain continuous flow across workflows

Choosing the Right Robotic Picking Automation

Talk to a Logistics Automation Expert

A logistics automation specialist will follow up to review your operations, workflows, and fulfillment challenges. The goal is to understand your setup and identify practical automation opportunities to improve efficiency and scalability—no commitment required.