<link rel="stylesheet" href="styles-JUTMGXX3.css"> Skip to main content

Robotic Kitting + Packing

Achieve a more stable operation with predictable cycle times, reduced error rates, and the ability to scale without adding labor.
https://a.storyblok.com/f/169662/2058x2562/1cc7a16562/09_2021_casestory_evcoplastics_-24.jpg

Flexible Kitting and Packing with Robotics

Variability and inefficiencies are at their highest at the end of the fulfillment chain. Manual kitting + packing processes struggle to keep up with order customization, fluctuating volumes, and labor availability. Errors at this stage directly impact customer satisfaction and returns, making consistency and traceability critical.

Universal Robots commercial graded collaborative robots (cobots) combined with MiR autonomous mobile robots, enable a flexible, scalable approach commercially. Instead of fixed automation, operations can deploy modular workcells that adapt to changing SKUs, order profiles, and throughput requirements. Cobots handle repetitive picking, sorting, and packing tasks with precision, while AMRs keep workstations supplied and move completed kits efficiently downstream.

Kitting and packing environments demand flexibility and consistency at the same time. Traditional automation struggles to deliver both. Cobots and AMRs are designed for this exact operating model.

  • Flexible automation for mixed-SKU operations: Adapt quickly to changing order profiles without retooling
  • Rapid deployment and reconfiguration: Implement cells in weeks, not months
  • Scalable architecture: Add robots or stations as demand increases without redesigning the system
  • Minimal infrastructure requirements: Operate without fixed conveyors or major layout changes
  • Continuous material flow: AMRs keep workstations supplied and remove bottlenecks
  • Reduced manual handling: Minimize non-value-added movement and repetitive tasks
  • Safe human-robot collaboration: Deploy directly alongside workers without extensive guarding
Case Story EVCO Plastics

Why Cobots and AMRs for Kitting + Packing

Traditional automation requires predictable product flow and long payback cycles, limiting its use in dynamic fulfillment environments. Collaborative robots and autonomous mobile platforms provide a different model—one built for variability.

Universal Robots cobots deliver precise, repeatable handling for mixed-SKU operations and can be quickly redeployed as requirements change. MiR AMRs extend this by managing material movement across the operation, eliminating delays between process steps and ensuring continuous flow.

Together, they create a connected system where workstations stay productive and material moves without interruption.

Designed for Real Warehouse Conditions

Kitting + packing environments are not controlled production lines—they are dynamic, often constrained by space, labor, and fluctuating demand. Solutions need to work within those constraints. Cobot-based cells are compact and easily reconfigured, allowing them to be deployed directly into existing pack lines or as standalone stations. AMRs operate alongside people and equipment, dynamically adjusting routes without fixed infrastructure.

This allows operations to improve performance without large capital projects or extended downtime.

Choosing the Right Robotic Kitting + Packing Automation

Talk to a logistics automation expert

A logistics automation specialist will follow up to review your operations, workflows, and fulfillment challenges. The goal is to understand your setup and identify practical automation opportunities to improve efficiency and scalability—no commitment required.