Articles Download Safety & Security Forum myUR Go to Main Site

Universal Robots A/S
Energivej 51
DK-5260 Odense S

T: +45 8993 8989
sales@universal-robots.com

 
  • Articles
  • Download
  • Safety & Security
  • Forum
  • myUR
  • Go to Main Site
  • Support
  • Articles
  • ActiNav - Re-grip logic and Sample Progam

ActiNav - Re-grip logic and Sample Progam

Adding standard Polyscope Waypoints to the End of a Bin Picking Sequence

Last modified on Feb 24, 2022

Introduction

Polyscope Waypoints can be combined with an ActiNav bin picking program to implement Polyscope palletizing, re-grip fixtures, and others.  This TechNote gives an example of a program that sometimes moves a part directly to a placement fixture, and sometimes to a re-grip fixture.

Rules

For bin picking, the ActiNav Autonomous Motion Module (AMM) plans all of the robot movements.  Standard Polyscope Waypoints cannot be freely mixed in with the ActiNav logic inside of the ActiNav Pick and Place loop.  But it is possible to switch to Polyscope movements and then back to ActiNav at the end of a Pick and Place loop.  The rules are:

  • The last pose of the robot after placement must be set by an ActiNav Custom Pose. This must be of the Type Robot Pose.
  • The first Waypoint in Polyscope must be the identical robot pose.
  • After Polyscope commands are complete, the robot must be returned to the first Waypoint, the one that was the same as the last Custom Pose.

 

Example Program

Please refer to the figure below:

  1. This program has two pick and place rules. One of them moves the part to the final placement fixture, and the other moves the part to a re-grip fixture.  Once the pick and place sequence has ended, the program must detect whether the part is in the re-grip fixture, and if so, move it to the final placement fixture, using standard Polyscope programming.
  2. A Custom Pose in robot coordinates moves the robot to some position that is convenient to both the re-grip fixture and the final placement fixture, since the robot could have been in either position before this. The AMM will move to the Custom Pose with full collision avoidance and path planning.
  3. An IF statement detects whether there is a part in the re-grip fixture or not. In this case, a binary sensor is used.  If there is a part in the re-grip fixture, it must be moved to the final placement fixture in steps 4 - 6.
  4. To switch to Polyscope control of the robot, the first Waypoint is identical to the ActiNav Custom Pose. This is the handoff of control.
  5. The part is moved from the Re-grip fixture to the final placement fixture with standard Polyscope programming.
  6. To switch back to ActiNav control of the robot, the robot is returned to the previous Custom Pose position by sending it to the same waypoint as in step 4.
  7. Control is returned to ActiNav. The pick & place loop ends, and the next pick is executed.

 

Related articles

Palletizing with ActiNav
ActiNav Rescan - Sample Program
Sample ActiNav Program
logo

Product

  • UR3e Robot
  • UR5e Robot
  • UR10e Robot
  • UR16e Robot
  • UR20 Robot
  • UR+ Products

Company

  • About us
  • Contact us
  • Careers We're hiring
  • UR merchandise

Training / Resources

  • Academy
  • Technical Resources
  • Articles
  • FAQ

Insights

  • Blog
  • Content library
  • News centre
  • Podcast
  • Webinars & Events

Get in touch

  • Ask an Expert
  • Schedule a no-cost assessment
  • Find a distributor
  • Customer support

Connect with us

  • LinkedIn
  • Facebook
  • Twitter
  • YouTube
  • Instagram
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com
  • Copyright @ Universal Robots 2026
  • Cookie policy
  • Privacy policy
  • Universal Robots A/S
  • Energivej 51
  • DK-5260 Odense S
  • T: +45 89 93 89 89
  • sales@universal-robots.com
  • US Corporate Office
  • 27-43 Wormwood St.
  • 02210 Boston, MA.
  • +1-844-GO-COBOT
  • ur.na@universal-robots.com

Copyright © Universal Robots 2026

Cookie policy
Privacy policy