Dual Robot Calibration
| 描述 |
Dual Robot Calibration calibrates the robot in the full work space. Each new robot is Dual Robot Calibrated as part of final assembly. If a joint is replaced on a calibrated robot the calibration is no longer valid.
Performing a Dual Robot Calibration after replacement of a joint allows the robot to continue in the production line without modifying waypoints in the robot program. To perform a Dual Robot Calibration, you need:
You can download the Calibration Manual from the Universal Robots Support site www.universal-robots.com/support/
|