| Footer Icons
|
| Icon
|
Title
|
Description
|
|
|
Initialize |
Manages the robot state. When RED, press it to make the robot operational.
-
Black, Power off. The robot arm is in a stopped state.
-
Orange, Idle. The robot arm is on, but not ready for normal operation.
-
Orange, Locked. The robot arm is locked.
-
Green, Normal. The robot arm is on and ready for normal operation.
-
Red, Error. The robot is in a fault state, such as Emergency Stop.
-
Blue, Transition. The robot is changing state, such as brake releasing.
|
|
Play
|
Starts the current loaded program. |
|
Step
|
Allows a program to be run single-stepped. |
|
Stop
|
Halts the current loaded program. |
|
Speed Slider
|
Shows in real time the relative speed at which the robot arm moves, taking safety settings into account. |
|
High Speed Manual Mode
|
The High Speed Manual slider is only available in manual mode when a Three-Position Enabling Device is configured. High Speed Manual Mode allows tool speed and elbow speed to temporarily exceed the default speed limit. |
|