Force Mode
| Description |
The Force Mode command enables you to set force and speed limits in the X, Y, Z, RX, RY, and RZ directions. Use it when you need to control contact force or a torque about an axis, rather than hold an exact pose on that axis. Apply it when you push, pull, roll along a surface, or follow a path while applying a side force. If nothing contacts a compliant axis with a non-zero wrench, the arm accelerates along that axis to the configured speed limit.
|
|
To access the Force Mode command |
|
|
Follow and Feature Frame fields |
In the Follow field, select one of three modes: Point, Motion, or Frame.
|
||||
|
|
In the Feature Frame field, select:
|
|
Setup panel |
|
|
Tuning panel |
Tap Tuning, then use the Gain, Damping, and Zero sensor functions.
|