The Calibration Horse

Description

The Calibration Horse connects one robot arm to another via the base, as illustrated in the image below. Using the Calibration Horse allows you to attach the two tool flanges. The result is a closed robot arm circuit that makes coordinated movements while performing a number of measurements.