Tool Drawings
| Description |
Two calibration mounts are available.
The calibration kit (185500) includes a smaller calibration horse and can be used with the following robots: All e-Series robots.
The calibration kit (200977) includes a larger calibration horse and can be used with the following robots: UR10e, UR16e, and UR Series robots.
|
| Calibration Horse (185500) Only e-Series |
The UR3e and the UR10e robot arms are mounted in different positions.
|
| Calibration Connector (185500) Only e-Series |
|
| Calibration Horse (200977) UR10e, UR16e and UR Series |
|
| Calibration Connector (200977) UR10e, UR16e and UR Series |
|