Compute Module
| Description |
AI Accelerator includes Compute module based on NVIDIA Jetson Orin.
Read the NVIDIA Jetson Orin manual and follow all safety instructions.
|
| Compute Module position |
When positioning the Compute Module, ensure the following:
|
| Connecting Compute Module |
The Compute Module network connections are pre-configured with Lan1 designated for connecting to the robot's Control Box and Lan2 available for optional Internet connection.
Connect the port marked Lan1 on the Compute Module directly to the robot's Control Box with an Ethernet cable. Do not use router or switch.
|