Intended Use

Description

The AI Accelerator is intended to create robot applications using Pereception, AI and PolyScope X integraton solution.

 

Possible applications of AI Accelerator are limited by combination of the technical specifications of it's components. Consult technical specification of individual components to determine their suitability for a purpose.

 

For details about the conditions under which the robot should operate, see Declarations and Certificates and the technical specifications in the robot User Manual.

 

All UR robots are equipped with safety functions, which are purposely designed to enable collaborative applications, where the robot application operates together with a human. The safety function settings must be set to the appropriate values as determined by the robot application risk assessment.

 

Collaborative applications, without guards or protective devices, are only intended for non-hazardous applications, where the complete application, including tool/end effector, work piece, obstacles and other machines, is low risk according to the risk assessment of the specific application.

The AI Accelerator shall not be used with CB3 robots or PolyScope versions prior to 10.11.1.

  • Only use AI Accelerator with UR e-Series robots running PolyScope X 10.11.1 or later.

Using UR robots or UR products outside of the intended uses can result in injuries, death and/or property damage. Do not use the UR robot or products for any of the below unintended uses and applications:

  • Medical use, i.e. uses relating to disease, injury or disability in humans including the following purposes:

    • Rehabilitation

    • Assessment

    • Compensation or alleviation

    • Diagnostic

    • Treatment

    • Surgical

    • Healthcare

    • Prosthetics and other aids for the physically impaired

    • Any use in proximity to patient/s

  • Handling, lifting, or transporting people

  • Any application requiring compliance with specific hygienic and/or sanitation standards, such as proximity or direct contact with food, beverage, pharmaceutical, and /or cosmetic products.

    • UR joint grease can be released into the air (vapor), or drip.

  • Any use, or any application, deviating from the intended use, specifications, and certifications of UR robots or UR products.

  • Misuse is prohibited as the result could be death, personal injury, and /or property damage

UNIVERSAL ROBOTS EXPRESSLY DISCLAIMS ANY EXPRESS OR IMPLIED WARRANTY OF FITNESS FOR ANY PARTICULAR USE.

  • The AI Accelerator is designed for use in standard industrial environments and is sold “AS-IS”. Universal Robots makes no declaration of conformity, claim of functionality, or fitness for particular purpose to the extent the AI Accelerator is used beyond the prescribed intended use.

  • The user shall ensure that the AI Accelerator is at all times used in full compliance with all applicable regulatory and legal requirements. If the user utilizes the AI Accelerator for applications outside the intended use, the user shall bear sole and exclusive liability.

Failure to use the AI Accelerator in accordance with the intended use can result in unsafe situations.

  • Read and follow the recommendations for intended use provided in this manual.