Operating Environment

Description

Special precautions should be taken when using components of the AI Accelerator in industrial environment.

 

Consider summary of the factors, such as ingress prevention rating for each of the components, the airflow requirements and ambient temperature range. See Technical Specifications and Technical Specifications section in Robot User Manual.

Failure to follow any of the below can result in serious injury or death due to electrical hazards.

  • Make sure all equipment not rated for water exposure remain dry. If water is allowed to enter the product, lockout-tagout all power and then contact your local Universal Robots service provider for assistance.