Script Files

Description

Script files are used in the program through the Script Node, imported from a disk into PolyScope X. The script files are managed via the System Manager

 

To access Script Files
  1. Navigate to the System Manager by tapping either the System Manager or header.

  2. Tap Script Files in the left column, and add your script file + Script File. The file on disk should have the .script extension.

     

Script files are kept according to their file name. So reimporting the script file again from disk will overwrite the old one. Once imported, the script file can be deleted or viewed.