set_standard_analog_out(n, f)
Set standard analog output signal level
Parameters
n: The number (id) of the output, integer: [0:1]
f: The relative signal level [0;1] (float)
Example command: set_standard_analog_out(1,1.0)
- Example Parameters:
- n is standard analog output port 1
- f = 1.0, that corresponds to 10V (or 20mA depending on domain setting) on the output port