get_standard_digital_out(n)
Get standard digital output signal level
See also get_configurable_digital_out and get_tool_digital_out.
Parameters
n: The number (id) of the output, integer: [0:7]
Return Value
boolean, The signal level.
Example command: get_standard_digital_out(1)
- Example Parameters:
- n is standard digital output 1
- Returns True or False
- n is standard digital output 1