get_standard_digital_in(n)

Get standard digital input signal level

See also get_configurable_digital_in and get_tool_digital_in.

Parameters

n: The number (id) of the input, integer: [0:7]

Return Value

boolean, The signal level.

Example command: get_standard_digital_in(1)

  • Example Parameters:
    • n is standard digital input 1
      • Returns True or False