get_standard_analog_in(n)

Get standard analog input signal level

See also get_tool_analog_in.

Parameters

n: The number (id) of the input, integer: [0:1]

Return Value

float, The signal level in Amperes, or Volts

Example command: get_standard_analog_in(1)

  • Example Parameters:
    • n is standard analog input 1
      • Returns value of standard analog input #1