rtde_set_watchdog(variable_name, min_frequency, action=’pause’)
This function will activate a watchdog for a particular input variable to the RTDE. When the watchdog did not receive an input update for the specified variable in the time period specified by min_frequency (Hz), the corresponding action will be taken. All watchdogs are removed on program stop.
>>> rtde_set_watchdog("input_int_register_0", 10, "stop")
Parameters
variable_name: Input variable name (string), as specified by the RTDE interface
min_frequency: The minimum frequency (float) an input update is expected to arrive.
action: Optional: Either "ignore", "pause" or "stop" the program on a violation of the minimum frequency. The default action is "pause".
Return Value
None
Note: Only one watchdog is necessary per RTDE input package to guarantee the specified action on missing updates.
Example command: rtde set watchdog( "input int register 0" , 10, "stop" )
- Example Parameters:
- variable name = input int register 0
- min frequency = 10 hz
- action = stop the program