Non-stop robot precision for 7 years: Cobots deliver the last "Magic 5%" in swim goggle production
By automating the final "magic 5%" of production - the precise trimming of swim goggles’ silicone gaskets based on individual face scans - UR cobots allow THEMAGIC5 to deliver affordable, custom-fit goggles. Universal Robots provided the only platform nimble and flexible enough to integrate with THEMAGIC5's proprietary software and durable enough to sustain non-stop production for more than 7 years, enabling the company to scale from a Kickstarter sensation to selling over 400,000 goggles worldwide.