BWIndustrie, the French manufacturer that has deployed the world 1st #UR16e
4 robotic arms from Universal Robots (one UR5, two UR10 and one model of the new UR16e) are deployed on production lines. The cobots handle tasks such as loading and unloading of #CNC lathes, quality control of metallic tubes and deburring of metal parts ranging from 4 to 14 kg. Using cobots from Universal Robots enables BWIndustrie to maintain #competitiveness and increase its #workforce by 50% and #revenues by 70%. The company has also been able to #reduce the risk of musculoskeletal disorders (MSDs) among employees, ensuring a healthier working #environment.