作業用移動

説明

The Process Move command enables you to program a linear movement with constant speed through a number of points. You must set blend radius to make sure that the robot moves at a constant speed between each move node. You can specify a reference frame and a transform pose.

 

To access Process Move command
  1. Go to the main program screen. 「Command Nodes」を参照してください。

  2. Tap the Process Move icon in the Commands toolbox.

     

    A node is inserted into the program tree. The node has three editable fields, Edit Point button, and ellipsis icon.

    These are the three fields:

    • 動作プロファイル

    • 名前

    • ブレンド

 

  1. In the Motion Profile field, you can choose either Custom or Process.

    Custom motion profile enables you to define movement data in Joint Move and Linear Move nodes.

    Process motion profile is a predefined motion in Joint Move and Linear Move nodes.

  2. Tap the Name field.

    Three tabs appear:

    • 値

    • 変数

    • 式

  3. Enter data in the Value, Variable, and Expression tabs, and tap Confirm. See Value-Variable-Expression Tabs.

  4. Tap Edit Point.

    A new screen appears with the robot arm interface.

  5. Tap the Blend field.

    Three tabs appear:

    • 値

    • 変数

    • 式

  6. Enter data in the Value, Variable, and Expression tabs, and tap Confirm. See Value-Variable-Expression Tabs.

 

移動ノードのモーションプロファイルラベル

プログラムツリー内のすべての移動関連コマンドノードには、各ノードに関連付けられた移動プロファイルが表示されます。 この機能により、移動ノードで選択されている移動プロファイルを確認できます。 この機能は以下のコマンドノードに実装されています:

カスタムモーションプロファイルを使用する移動ノードでは、モーションプロファイルの代わりに速度と加速度の値が表示されます。

 

 

To use More Option

  1. Tap the ellipsis icon.

    More settings screen appears with three settings:

    • 動作

    • 基準

    • 変換

  2. Tap the Movement setting on the left side.

    A Motion Profile field with selections Custom and Process is on the right side.

  3. If Custom is selected, a Speed field and Acceleration field appears.

  4. Tap the Speed field, and the Value, Variable, and Expression tabs pop up.

  5. Enter data in each tab, and tap Confirm. See Value-Variable-Expression Tabs.

  6. Tap the Acceleration field, and the Value, Variable, and Expression tabs pop up.

  7. Enter data in each tab, and tap Confirm. See Value-Variable-Expression Tabs.

  8. Choose Process motion profile and tap Confirm.

  9. Tap the Reference setting.

  10. Choose either Frame or Set TCP field.

  11. In the Position column, tap the X, Y, Z tab and enter your chosen value for the robot, and Confirm.

  12. In the Rotation column, tap the RX, RY, RZ tab and enter your chosen value for the robot, and Confirm.

  13. In the Transform setting, tap the Pose field and Confirm.