transpose(m)
Get the transpose of a matrix
Parameters
m: matrix or an array
Return Value
transposed matrix or array
Example command:
transpose([[1,2],[3,4],[5,6]]) -> Returns [[1,3,5],[2,4,6]]
transpose([1,2,3]) -> Returns [[1],[2],[3]]
transpose([[1],[2],[3]]) -> Returns [1,2,3]