log(b, f )
Returns the logarithm of f to the base b
Returns the logarithm of f to the base b. If b or f is negative, or if b is 1 a runtime error is raised.
Parameters
b: floating point value
f: floating point value
Return Value
the logarithm of f to the base of b.
Example command: log(10.,4.)
- Example Parameters:
- b is base 10
- f is log of 4
- Returns 0.60206