Introduction
| The Realtime communications Interface |
| (The RealTime interface has been deprecated since version 3.5. It is recommended to use the RTDE Interface, instead) |
| The information on this section applies to UR software versions shown, below: |
| RealTime client=port 30003 |
| RealTime client read only=port 30013 |
| The realtime communications interface is also known as the Matlab interface |
| e-Series (500 Hz): |