TCP Orientation
| Description |
The new TCP orientation wizard provides a convenient way of determining the orientation (rotation) of a TCP. By having the user move the robot to a position where the tool's Z-axis aligns with a selected frame, the wizard can compute the TCP orientation automatically.
|
|
TCP Orientation wizard |
|
|
|
|
| Pose representation |
PolyScope X and the ROS 2 interface provide the same TCP pose. The TCP orientation is also the same, but different mathematical representations are used. Therefore, the values are not directly comparable.
|
and the pop-up TCP Orientation Measurement screen appears.