Configuration Settings

Description

The settings in PolyScope X can be accessed via the hamburger menu in the main navigation.

You can access the following sections: 

  • General

  • Password

  • Connection

  • Security

 

General Settings

In the general settings, you can change the preferred language, units of measurements, etc. You also update the software from the general settings.

Password Settings

In the password settings, you can find the default passwords, and how to change them to the preferred and secure passwords.

Connection Settings

In the connection settings, you can set network settings such as IP address, DNS server, etc. Settings related to UR Connect is also found here.

Security Settings

The security settings related to SSH, admin password permissions and enabling/disabling of various services in the software.