Restoration of Recovered Image Files
| Description |
To restore recovered robot image files, a Linux file support system is needed, the same as in data recovery.
|
|
Re-imaging using Linux command |
This is an optional process. Users who successfully recovered and re-imaged robot file should implement this procedure.
To re-image a recovered file, a Linux command such as this can be used:
sudo dd if="/path/to/ursys-CB5.0-5.24.0-build12.19.432-secure.img" of=/dev/sdb bs=4M status=progress
Where:
|