USB Update Procedure

Prerequisites

This procedure requires a USB storage device that is detectable by Windows and is FAT32 formatted.

 

If the storage device is not FAT32 formatted, perform the following procedures:

  • You might need admin privileges to perform the procedure.

  • Back up any important data on the USB storage device before formatting. The process will erase all existing information.

  1. Connect the USB to your computer.

  2. Open File Explorer.

  3. Right-click on the USB drive and select Format.

  4. In the format window, select Restore device defaults.

  5. In the Volume label, specify the robot's product line as shown in the following table.

    e-Series and UR Series Generation 3
    Standard G3
    UR20 CB3
  6. Select Start to begin formatting.

  7. Confirm any warning messages.