Image Installation and Re-imaging into USB Drive
| Description |
A bootable USB enables users to boot a control box with a new robot image in either Polyscope 5 or Polyscope X software version, in case of emergency situation when a robot's internal storage gets damaged.
|
| Installing image using balenaEtcher |
If your USB flash drive was previously formatted as Windows partition, it will be fully erased, and partition type is changed to ext3 and ext4 making it unreadable for Windows. If Linux file system support is not installed, you have no way to access the USB flash drive.
|
| Robot Image into USB |
|
|
|
|
|
|
|
|
|
|
|