Dual Robot Calibration
Dual Robot Calibration calibrates the robot in the full work space. Each new robot is Dual Robot Calibrated as part of final assembly.
Performing a Dual Robot Calibration after replacement of a joint allows the robot to continue in the production line without modifying waypoints in the robot program.
To perform a Dual Robot Calibration, you need:
- 2 robots (same size and same generation)
- Dual Robot Calibration Tooling Complete (Part no: TBD)
You can download the Calibration Manual from the Universal Robots Support site www.universal-robots.com/support/