Assembling Clamp Connection

Clamp assembly

The assembly is done in reverse of the disassembly. However, a few things must be noted before assembly is begun.

• Always replace the flexible flat black ring with a new one to maintain the IP classification.
• Replace the foam seal on the clamps, if damaged, to maintain the IP classification.
• Replace the wear rings if extensive wear or damage is shown.
• The dots must be aligned; otherwise, the connection cannot be made.


• Joints should be assembled in a vertical position to ensure proper mating between the joints.
 


• Ensure the screws are inserted in the correct clamp.

• Apply only to earlier version of brackets where one side has a circular marker.

 

When tightening the clamps, it must be done in steps. Do not exceed recommended torque:

Step 1: Tighten one side so there is a gap of 1.0mm to 1.5mm.

Step 2: Tighten the other side completely with 5.0Nm. +/- 0.50 Nm.

Step 3: Tighten the first side with 5.0Nm. +/- 0.50 Nm.

Step 4: Ensure same gap at both ends.